정전은 플라스틱 포장재를 제조하는 기계에 값비싼 결과를 초래할 수 있습니다. 대표적인 예가 Windmöller & Hölscher의 Tiratex 포장 시스템입니다. 전기가 없으면 드라이브가 멈추고 발열체가 고장날 것입니다. 이로 인해 서로 달라붙은 기계 부품은 생산을 다시 시작하기 전에 힘들게 청소해야 합니다. 결과적으로 몇 시간 동안 지속되는 값비싼 생산 손실이 발생합니다. 무정전 전원 공급 장치(UPS)가 이러한 상황을 해결합니다. 인클로저 기술을 위한 시스템 제공업체인 Rittal은 UPS 전문업체 Wöhrle Stromversorgungssysteme와 산업용 에너지 저장 솔루션을 위한 솔루션 제공업체인 Commeo가 기계 제조업체를 위해 산업용 UPS를 구현한 기반을 제공합니다. 협력의 결과는 중단 없는 작동을 보장하는 모듈식 리튬 이온 에너지 저장 시스템을 갖춘 온라인 UPS 시스템의 개발입니다.
Works everywhere: The energy storage solutions from Rittal and Commeo can be used across a wide range of industries and applications. Their modularity ensures an uninterruptible power supply for mission-critical applications in, for example, the IT industry or in high-tech manufacturing processes. Power grid fluctuations can be compensated for by means of their battery buffer and by shifting energy storage and supply over time. Due to their high energy and power density, energy storage systems are also suitable for charging infrastructures in e-mobility or transport applications that use mobile robots or automated guided vehicles (AGVs). By using climate control solutions from Rittal, the energy storage units can also be used outdoors without any problems. Stainless steel housings also make other applications possible, e.g. in food production and processing.
Application examples:
- Uninterruptible Power Supply (UPS): The energy storage system from Rittal and Commeo provides the necessary energy in the event of a power failure, thereby creating economic security for companies.
- Peak shaving: A battery storage system designed to precisely meet individual requirements compensates for voltage peaks and can pay for itself in a short time thanks to the resulting lower energy supply costs.
- Charging infrastructure: If an extended grid connection is not possible or economical for electricity charging stations, a battery system offers a viable alternative to increase charging capacity and optimise the energy infrastructure.
Versatility guaranteed: With solutions from Rittal and Commeo, energy storage really gets into gear. The modular, flexible construction system enables simple installation of any energy storage unit in Rittal’s industrial or IT racks. Even large storage challenges are no problem, as several racks right up to containers can be linked and connected together to form a high-performance solution. The result: tailor-made outcomes.
VX25: The platform – from enclosures to cooling
Full industrial compatibility and suitability are the main reasons why the VX25 enclosure system was always going to be used as the basis for Commeo’s energy storage systems. However, there are even more benefits. With a load capacity of 1,500 N, even heavy components can be installed into the frame without any problems. As the frame section has a 25 mm pitch pattern both vertically and horizontally, enclosure expansions are extremely flexible, even beyond the enclosure’s limits. Given the range of enclosure sizes and the option of baying, the enclosures can be scaled up as needed. The protection category is IP 55 as standard, which is ideal if, for example, the energy storage systems are to be installed in harsh environmental conditions. If climate control of the energy storage unit is required, Rittal offers solutions perfectly designed for the specific enclosure system. The use of the compact and test-approved RiLine power distribution system and an IoT connection ensures ideal system monitoring can be put in place for the battery infrastructure.
Further links to Commeo:
Rittal and Commeo: Energy storage for online UPS
As well as charging infrastructures for e-mobility, joint solutions are also available for the emergency power supply of critical production facilities. One such example is the use of energy storage as an uninterruptible power supply in the plastics processing machinery of Windmöller & Hölscher.
Power cuts are a pain and costly, particularly when they bring machines and production to a standstill and can only be recommissioned after complex re-start programmes and costly cleaning processes. An emergency power solution can prevent such horror scenarios. Commeo and Rittal have worked together in an effort to develop a solution for an uninterruptible power supply. Rittal, as a supplier of enclosure system technology, provides the basis on which Commeo, the solution provider for industrial energy storage applications, has built and installed an industrially compatible UPS for the customer: Windmöller & Hölscher, a mechanical engineering company. This collaboration has produced an online UPS system with a modular lithium-ion energy storage unit that ensures a stable and continuous operation.
Rittal의 인클로저 시스템을 기본으로
Commeo는 에너지 저장 시스템의 개발과 함께 산업에 적합한 시스템을 구현하기 위해 완전히 새로운 접근 방식을 적용했습니다. Commeo의 상무이사인 미하엘 슈나켄베르크(Michael Schnakenberg)는 필수 요구 사항을 설명하면서 "완성된 시스템이 모든 일반적인 산업 표준을 충족하는 방식으로 리튬 이온 배터리를 전체 시스템에 통합하고 싶었습니다."라고 말합니다. 이것이 바로 이 회사가 예를 들어 인클로저 기술을 위해 Rittal의 VX25 인클로저 시스템에 의존하는 이유입니다. 또한 Wöhrle와 같은 시스템 통합업체도 전력 전자 장치를 Rittal 인클로저에 수용합니다. 시스템은 모듈식으로 설계되었으며 개별 배터리 셀과 배터리 관리 시스템이 수용되는 개별 에너지 저장 블록으로 구성됩니다. 이는 필요에 따라 확장할 수 있습니다. 이를 위해 필요한 수의 에너지 저장 블록이 VX25 인클로저에 제어 장치와 함께 설치됩니다.
시장 리더인 Rittal의 인클로저 시스템은 업계에서 확고한 입지를 구축했으며 우리의 에너지 저장 시스템이 시장에서 높은 수준의 수용을 이끌어냈습니다.
슈나켄베르크는 "다른 공급업체와 달리 우리는 에너지 저장 블록을 냉각하기 위해 수냉식을 사용하지 않습니다."라고 설명합니다. "즉, 유지 보수가 전혀 필요 없고 고장 가능성이 적습니다." 개별 블록에는 알루미늄 하우징에는 냉각 핀만 있습니다. 열 관리는 인클로저의 공조 시스템을 통해 이루어집니다. 그런 다음 공조 솔루션은 에너지 저장 시스템의 크기와 설치 장소의 주변 조건에 따라 조정할 수 있습니다. 여기에서도 Commeo는 시스템 파트너인 Rittal의 이점을 누립니다. 인클로저와 공조 시스템이 단일 소스에서 제공되므로 모든 것이 완벽하게 조정됩니다. "또한 우리는 공조 시스템과 관련하여 업계에서 입증된 시스템의 이점을 누리고 있습니다."라고 슈나켄베르크는 확고하게 말합니다.
세계 최초: 리튬 이온 기술이 적용된 산업용 UPS
미하엘 슈나켄베르크는 "이것은 산업 설비를 위한 세계 최초의 리튬 기반 무정전 비상 전원 공급 장치입니다"라고 자랑스럽게 말합니다. UPS는 1제곱미터 미만의 설치 공간에서 200kW의 출력으로 최대 6C의 방전 용량을 제공하는 모듈식 에너지 저장 블록으로 구성됩니다. 이 성능 데이터를 통해 시스템은 예를 들어 디젤 발전기가 시동되고 발전기가 공급을 인수할 때까지 위에서 언급한 Tiratex 포장 시스템 Windmöller & Hölscher에 대한 에너지 공급을 유지할 수 있습니다.
Real-world test
Power cuts are something Windmöller & Hölscher, manufacturers of flexible packaging machinery, cannot afford. If their high-tech systems come to a standstill, hours of production downtime are the consequence. With the joint solution from Rittal and Commeo, however, such power cuts will be a thing of the past in the future. For example, Windmöller & Hölscher’s TIRATEX tape stretching system is supplied with uninterruptible power.