Decision-making aid

How do I find the appropriate climate control solution?

To carry out complex production processes, sensitive and increasingly high-performance components are installed in enclosures. Selecting the right climate control solution is vital so as to ensure a long service life.

But what is the best climate control method for your system?

Could it be liquid cooling with an air/water heat exchanger, or cooling using a cooling unit or ambient air? Or perhaps you require enclosure heating. A holistic approach is needed to find the appropriate energy-efficient climate control solution for your system, because there are numerous aspects to consider. What are the ambient conditions at your system’s location, for example? Is it humid? Dusty? Hot? And what are the actual requirements in terms of cooling output?

Factors such as the type of installation (free-standing or integrated), the heat dissipation (passive or active) and the permissible noise level also need to be taken into account.

Did you know...

... that correct climate control can significantly lengthen the service life of components located in the enclosure?

The growing packing density in enclosures can lead to a huge increase in the heat loss!

As a general rule of thumb, a 10 °C rise in operating temperature halves the service life and doubles the failure rate.

Field study

Rittal conducted a field study on around 400 installations to investigate how climate control solutions are typically installed in industrial applications. This revealed a large number of failings that could have been prevented through optimum planning with the right tools.

To optimise the performance of climate control solutions, while also minimising their energy consumption, climate control needs to be planned correctly.

Typical failings resulting from incorrect climate control:

  • In 64% of installations, the warm components were not located in the air stream between the inlet and outlet of the climate control unit
  • 50% of the units examined have a capacity utilisation of less than 20%
  • In 93% of installations, no targeted cold-air circulation was envisaged/installed
  • 40% of units had heavily soiled filter mats and inadequate maintenance
  • In 18% of installations, the climate control unit’s inlet or outlet was obstructed in some way
  • 19% of installations had air short-circuits

Overview of types of climate control based on ambient conditions

The different types of climate control have a variety of features and offer a wide range of benefits.

Units for cooling with ambient air are ideal for dissipating heat loads with excellent cost-efficiency. The pre-requisite is a relatively clean ambient air at a temperature that is lower than the desired temperature inside the enclosure.

Requirements:

  • Relatively clean ambient air

  • Ambient temperature lower than the desired temperature inside the enclosure

Benefits:

  • Particularly energy-efficient
  • Fast, cost-effective installation
  • No customer infrastructure required

Find out more

Cooling units keep the temperature inside the enclosure at a constant level, regardless of the ambient temperature. The air routing meets individual requirements. Two separate circuits prevent the ingress of dust into the enclosure.

Requirements:

  • Also suitable for use in warm or dusty ambient air
  • Ambient temperature at least as high as the desired temperature inside the enclosure

Benefits:

  • Two separate circuits prevent the ingress of dust into the enclosure
  • The temperature inside the enclosure is kept at a constant level
  • Excellent energy efficiency thanks to the innovative Blue e+ series of cooling units

Find out more

Efficient liquid cooling is used wherever a high cooling load is required – for example, in process and machine cooling or if using air/water heat exchangers to dissipate heat losses from enclosures. Spatial separation between cooling production and process cooling can be achieved with liquid cooling systems.

Requirements:

  • Also suitable for use in corrosive or oily ambient air
  • Ambient temperature can be higher or lower than the temperature inside the enclosure
  • A supply of cooling water must be ensured at the installation site

Benefits:

  • Exceptional temperature accuracy (constant water temperature)
  • Can cool both enclosures and machine tools
  • Suitable even for extremely high ambient temperatures
  • The heat exchanger and chiller can easily be kept separate, so no waste heat is generated in the room

Find out more

Condensation poses a particular risk for control electronics, especially with outdoor siting. Having a range of output categories ensures the correct thermal output is always available.

Requirements:

  • No requirements relating to the ambient air/temperature outside the enclosure

Benefits:

  • Distributes warm internal air evenly
  • Avoids subnormal temperatures in switchgear
  • Preventing condensation protects against corrosion

Find out more

Superbly coordinated components tailor the climate control components perfectly to your specific requirements – from targeted air routing and precise control of equipment to the appropriate consumables.

Benefits:

  • Monitoring, control and individual air routing can further increase the efficiency and reliability of climate control components

Go to product

Postcode

How can you reduce your carbon footprint and save hard cash?

Using energy-efficient enclosure and process climate control solutions can help. In many cases, it’s worth replacing older equipment with new, energy-efficient solutions.

Significant savings can be achieved in terms of both maintenance costs and energy consumption. As a result, the latest climate control solutions will definitely not be affected by the next stage of the EU regulation on fluorinated greenhouse gases and associated requirements.

 

Further videos:

1.6 kW Blue e+ cooling unit

Discover the benefits of the new performance calss for compact enclosure systems

Blue e+ chiller

Meet the world's most efficient range of chillers

Roof-mounted fan

Find out more about the operation and benefits of Rittal roof-mounted fans

Further downloads:

For efficient outdoor solutions
TopTherm Blue e wall-mounted cooling unit, UL type 3R/4

World's first
The e+ principle

Blue e+ roof-mounted cooling unit
VX25 integration solution

Blue e+ chiller
With the e+ principle

The digital upgrade for Blue e cooling units
Blue e IoT adaptor

High efficient needs- based cooling Blur e chiller
Blue e chiller

Based on the new NEC 2017
Machine approvals in North America

 

References

Bosch Rexroth

Fifty percent less energy consumption

You should never underestimate the energy consumption of machine tools: cooling enclosures and spindles for instance account for more than 15 per cent of it. A test installation in a CNC lathe at Bosch Rexroth demonstrated that the new Rittal Blue e+...

Xylem Services GmbH

Xylem Services GmbH cuts operating costs with Rittal Blue e+ cooling units

Xylem Services GmbH is saving an annual five-figure sum by using Blue e+ cooling units from Rittal to cool its switchgear.

Ford Motorenwerke

Service and efficiency check of cooling units reveals savings potentials

The Ford engine plant in Cologne was forced to shut down a number of times in the space of a year due to defective cooling units. The company immediately accepted the offer from Rittal to carry out a manufacturer-independent inventory of all cooling...