TX CableNet

Get IT. Locate IT. Patch IT.

The TX CableNet is “Simply. Perfection”. The new IT rack is the future-proof solution for all users who expect “best in class” functionality and total quality, i.e. a network rack which satisfies all requirements by covering all the bases. Rittal combines years of experience with extensive working knowledge of network infrastructures in this truly exceptional solution.

TX CableNet – YOUR BENEFITS

Rack concept + best practice

  • "Waterfall” cable routing principle with simple, secure cable routing from the roof
  • Roof concept also allows for retrospective fitting of a fan mounting plate for active rack ventilation
  • Also supports cable routing from below, for use in raised-floor situations
  • Safe cable laying while observing the critical cable bending radius
  • Simple fitting and removal of side panels and doors, plus rapid access to the inner rack area
  • More structure & order in the IT rack + protection of cabling and components

Portfolio + accessories

  • 13 rack options with location-variable cable routing as standard, with or without side panel
  • Efficient rack and frame design plus complete compatibility with TS & VX accessories
  • Vented doors with a 78% perforated surface are available for installation of active and passive network equipment
  • Removable cable routing strips for fast, tool-free access to the side rack areas

The portfolio

The choice is yours: One rack,
13 options

Roof plate with concealed cut-out for fan mounting plate

As IT manager, you have carefully planned your IT infrastructure and at the time of installation, do not require active cooling of your IT racks due to low capacity utilisation resulting from the interior configuration. Imagine a situation where demand has increased and more active components are being added to the rack. Suddenly, active cooling becomes more important. The TX CableNet has the answer, with its multi-functional roof plate. Direct installation or retro-fitting of a fan mounting plate instead of the covered cut-out in the roof plate can be easily achieved. Alternatively, with screw-fastened roof plate designs, the cover plate can be raised with spacers to encourage ventilation. Best of all, there’s no need to invest in a new IT rack.

The choice is yours: One rack,
13 options

Roof plate with concealed cut-out for fan mounting plate

As IT manager, you have carefully planned your IT infrastructure and at the time of installation, do not require active cooling of your IT racks due to low capacity utilisation resulting from the interior configuration. Imagine a situation where demand has increased and more active components are being added to the rack. Suddenly, active cooling becomes more important. The TX CableNet has the answer, with its multi-functional roof plate. Direct installation or retro-fitting of a fan mounting plate instead of the covered cut-out in the roof plate can be easily achieved. Alternatively, with screw-fastened roof plate designs, the cover plate can be raised with spacers to encourage ventilation. Best of all, there’s no need to invest in a new IT rack.

The choice is yours: One rack,
13 options

Roof plate with concealed cut-out for fan mounting plate

As IT manager, you have carefully planned your IT infrastructure and at the time of installation, do not require active cooling of your IT racks due to low capacity utilisation resulting from the interior configuration. Imagine a situation where demand has increased and more active components are being added to the rack. Suddenly, active cooling becomes more important. The TX CableNet has the answer, with its multi-functional roof plate. Direct installation or retro-fitting of a fan mounting plate instead of the covered cut-out in the roof plate can be easily achieved. Alternatively, with screw-fastened roof plate designs, the cover plate can be raised with spacers to encourage ventilation. Best of all, there’s no need to invest in a new IT rack.

The choice is yours: One rack,
13 options

Roof plate with concealed cut-out for fan mounting plate

As IT manager, you have carefully planned your IT infrastructure and at the time of installation, do not require active cooling of your IT racks due to low capacity utilisation resulting from the interior configuration. Imagine a situation where demand has increased and more active components are being added to the rack. Suddenly, active cooling becomes more important. The TX CableNet has the answer, with its multi-functional roof plate. Direct installation or retro-fitting of a fan mounting plate instead of the covered cut-out in the roof plate can be easily achieved. Alternatively, with screw-fastened roof plate designs, the cover plate can be raised with spacers to encourage ventilation. Best of all, there’s no need to invest in a new IT rack.

The choice is yours: One rack,
13 options

Roof plate with concealed cut-out for fan mounting plate

As IT manager, you have carefully planned your IT infrastructure and at the time of installation, do not require active cooling of your IT racks due to low capacity utilisation resulting from the interior configuration. Imagine a situation where demand has increased and more active components are being added to the rack. Suddenly, active cooling becomes more important. The TX CableNet has the answer, with its multi-functional roof plate. Direct installation or retro-fitting of a fan mounting plate instead of the covered cut-out in the roof plate can be easily achieved. Alternatively, with screw-fastened roof plate designs, the cover plate can be raised with spacers to encourage ventilation. Best of all, there’s no need to invest in a new IT rack.

TX CableNet conversion tool

We want to make it as convenient as possible for you to switch from the tried-and-trusted Rittal TE 8000 to its new and improved successor, the TX CableNet. With 13 options, including new sizes with space-optimised heights and depths tailored even more effectively to your future requirements, the TX CableNet maintains the tried-and-tested quality of its predecessor, while at the same time setting new standards.

What does the conversion tool do? Search for the Model Numbers of TE network racks and get a list of alternative racks with similar dimensions – if indeed you want to use exactly the same sizes. In some cases, VX IT will also be displayed here. Please check whether the recommendation is suitable for you and your application. You may well find that the brand new size variants of the TX CableNet are even more beneficial. Please note that previously installed accessories may deviate from this. You complete the conversion by creating and downloading a wish. Register or alternatively, please contact your local ASM or customer service team.

Rittal TE 8000Rittal TX CableNet/ VX IT
Model No. Designation Packs of Model No. Designation Packs of Info Wish list
Rittal TE 8000 Model No.7888.390 DesignationTE 8000 network rack, WHD: 600x600x600 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No. DesignationOld item, no successor Packs of InfoWish list
Rittal TE 8000 Model No.7888.410 DesignationTE 8000 network rack, WHD: 600x600x800 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No. DesignationOld item, no successor Packs of InfoWish list
Rittal TE 8000 Model No.7888.430 DesignationTE 8000 network rack, WHD: 600x1200x600 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.7888.276 DesignationTX CableNet, glazed door, 24 U, WHD: 600x1200x600 mm, RAL 7035, with side panels Packs of1 pc(s). InfoWish list
Rittal TE 8000 Model No.7888.440 DesignationTE 8000 network rack, WHD: 600x1200x800 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.7888.278 DesignationTX CableNet, glazed door, 24 U, WHD: 600x1200x800 mm, RAL 7035, with side panels Packs of1 pc(s). InfoWish list
Rittal TE 8000 Model No.7888.500 DesignationTE 8000 network rack, WHD: 600x2000x600 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.7888.266 DesignationTX CableNet, glazed door, 42 U, WHD: 600x2000x600 mm, RAL 7035, with side panels Packs of1 pc(s). InfoWish list
Rittal TE 8000 Model No.7888.510 DesignationTE 8000 network rack, WHD: 600x2000x800 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.7888.268 DesignationTX CableNet, glazed door, 42 U, WHD: 600x2000x800 mm, RAL 7035, with side panels Packs of1 pc(s). InfoWish list
Rittal TE 8000 Model No.7888.460 DesignationTE 8000 network rack, WHD: 800x1200x800 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.7888.218 DesignationTX CableNet, glazed door, 24 U, WHD: 800x1200x800 mm, RAL 7035, with side panels Packs of1 pc(s). InfoWish list
Rittal TE 8000 Model No.7888.430 DesignationTE 8000 network rack, WHD: 600x1200x600 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.5326.121 DesignationVX IT, solid, 19" mounting angles standard, RAL7035, WHD 600x1200x600mm, 24U Packs of1 pc(s). Info
Depending on how and where it is sited, the door opening angle may vary for selected applications
Wish list
Rittal TE 8000 Model No.7888.440 DesignationTE 8000 network rack, WHD: 600x1200x800 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No. DesignationOld item, no successor Packs of InfoWish list
Rittal TE 8000 Model No.7888.500 DesignationTE 8000 network rack, WHD: 600x2000x600 mm, with glazed door Packs of1 pc(s). Rittal TX CableNet/ VX IT Model No.5329.121 DesignationVX IT, solid, 19" mounting angles standard, RAL7035, WHD 600x2000x600mm, 42U Packs of1 pc(s). Info
Depending on how and where it is sited, the door opening angle may vary for selected applications
Wish list
Show 1 - 10 of 27 entries
Back123Next

Note: Mounted accessories may differ. For special queries, the VX IT configurator can help you find a suitable solution.

Application scenarios

Healthcare

The TX CableNet is ideal as a conventional network distributor. The new type of cable entry above the roof – based on the “waterfall” concept – allows for the critical bending radii of copper and fibre-optic cables and makes inserting and clamping even large volumes of cable simple. As part of the climate control concept, vented doors support a mix of active and passive network equipment, such as switches for grouping and distributing data. The cold air from the surrounding office air-conditioning system easily reaches the active components via the perforated front and rear doors. All relevant rack parameters are easily monitored from a Web browser with a CMC III monitoring system or smart power distribution units (PDUs) that can be extended with, for example, sensors. The connection to a building or IT management system enables the monitoring of the distribution infrastructure even in very large properties and buildings such as those found in the healthcare sector – for example, hospitals, clinics or other medical care facilities.

Healthcare – Well cared-for
Telcotry

As well as supporting the “waterfall” concept with user-friendly cable entry from above, the TX CableNet is also equally suitable for office environments with a raised floor. Cables are simply inserted from underneath the rack. In this sample application, the cables of all IT components such as PCs, telephones or printers are routed to the patch panels, grouped together via a switch, and forwarded to a central server. The glazed door of the TX CableNet provides a clear view of the rack interior at all times, enabling complete control of all components. Climate control is equally straightforward and reliable – the cold air from the surrounding office air-conditioning system easily reaches the active components via the perforated front and rear doors. These doors can be easily and safely cooled optionally via a retrofittable fan mounting plate in the roof panel prepared for this purpose. Additional security is provided by the optionally installed AX comfort handle with security lock to guard against unauthorised access.

Telco – Cable management made easy

Videos

Video presentation HM digital 2021 Transformation based on an innovative IT infrastructure – the new generations of racks to power.

Contact

Do you have questions about the TX CableNet? We’ll be happy to answer your questions on all aspects of the IT rack.

Consent to advertising

Possibility of revocation

Of course you can revoke your consent at any time with effect for the future. You can assert the revocation against Rittal GmbH & Co. KG via the following e-mail: info@rittal.com or contact the contact details provided in the imprint . Your revocation does not affect the legality of the processing of your data due to the consent until revocation. Further explanations on data protection at Rittal GmbH & Co. KG can be found at www.rittal.com/data-privacy

The fields marked with (*) are mandatory.