Strömavbrott kan få kostsamma konsekvenser för en maskin som tillverkar plastförpackningar. Ett typiskt exempel är Tiratex-förpackningsanläggningarna från Windmöller & Hölscher. Utan ström slutar både drivmotorer och värmeelement att fungera. Problem av det här slaget har fått maskindelar att fastna ordentligt, och måste rengöras mycket noga innan anläggningen kan startas igen. Resultat: Flera timmars dyrbart driftstopp. En avbrottsfri strömförsörjning (UPS) kan lösa det hela. Apparatskåpsleverantören Rittal står för grunderna till det industriklassade UPS-system som Wöhrle Stromversorgungssysteme och Commeo har tagit fram. Samarbetet resulterade i ett uppkopplat UPS-system med ett modulärt litiumjonbatteri som levererar avbrottsfri strömförsörjning.
Works everywhere: The energy storage solutions from Rittal and Commeo can be used across a wide range of industries and applications. Their modularity ensures an uninterruptible power supply for mission-critical applications in, for example, the IT industry or in high-tech manufacturing processes. Power grid fluctuations can be compensated for by means of their battery buffer and by shifting energy storage and supply over time. Due to their high energy and power density, energy storage systems are also suitable for charging infrastructures in e-mobility or transport applications that use mobile robots or automated guided vehicles (AGVs). By using climate control solutions from Rittal, the energy storage units can also be used outdoors without any problems. Stainless steel housings also make other applications possible, e.g. in food production and processing.
Application examples:
- Uninterruptible Power Supply (UPS): The energy storage system from Rittal and Commeo provides the necessary energy in the event of a power failure, thereby creating economic security for companies.
- Peak shaving: A battery storage system designed to precisely meet individual requirements compensates for voltage peaks and can pay for itself in a short time thanks to the resulting lower energy supply costs.
- Charging infrastructure: If an extended grid connection is not possible or economical for electricity charging stations, a battery system offers a viable alternative to increase charging capacity and optimise the energy infrastructure.
Versatility guaranteed: With solutions from Rittal and Commeo, energy storage really gets into gear. The modular, flexible construction system enables simple installation of any energy storage unit in Rittal’s industrial or IT racks. Even large storage challenges are no problem, as several racks right up to containers can be linked and connected together to form a high-performance solution. The result: tailor-made outcomes.
VX25: The platform – from enclosures to cooling
Full industrial compatibility and suitability are the main reasons why the VX25 enclosure system was always going to be used as the basis for Commeo’s energy storage systems. However, there are even more benefits. With a load capacity of 1,500 N, even heavy components can be installed into the frame without any problems. As the frame section has a 25 mm pitch pattern both vertically and horizontally, enclosure expansions are extremely flexible, even beyond the enclosure’s limits. Given the range of enclosure sizes and the option of baying, the enclosures can be scaled up as needed. The protection category is IP 55 as standard, which is ideal if, for example, the energy storage systems are to be installed in harsh environmental conditions. If climate control of the energy storage unit is required, Rittal offers solutions perfectly designed for the specific enclosure system. The use of the compact and test-approved RiLine power distribution system and an IoT connection ensures ideal system monitoring can be put in place for the battery infrastructure.
Further links to Commeo:
Rittal and Commeo: Energy storage for online UPS
As well as charging infrastructures for e-mobility, joint solutions are also available for the emergency power supply of critical production facilities. One such example is the use of energy storage as an uninterruptible power supply in the plastics processing machinery of Windmöller & Hölscher.
Power cuts are a pain and costly, particularly when they bring machines and production to a standstill and can only be recommissioned after complex re-start programmes and costly cleaning processes. An emergency power solution can prevent such horror scenarios. Commeo and Rittal have worked together in an effort to develop a solution for an uninterruptible power supply. Rittal, as a supplier of enclosure system technology, provides the basis on which Commeo, the solution provider for industrial energy storage applications, has built and installed an industrially compatible UPS for the customer: Windmöller & Hölscher, a mechanical engineering company. This collaboration has produced an online UPS system with a modular lithium-ion energy storage unit that ensures a stable and continuous operation.
Skåpsystem från Rittal som grund
När Commeo arbetade med att utveckla energilagringen valde man helt nya vägar för att utveckla ett system som passade industrisektorn. ”Vi ville definitivt bygga in litiumjonbatterierna i ett helhetssystem, men på ett sådant sätt att det färdiga systemet uppfyller alla gängse industristandarder”, säger Michael Schnakenberg, VD för Commeo, om ett av de väsentliga kraven. Det är därför företaget valde att använda skåp ur VX25-systemet från Rittal. Även systemintegratörer som Wöhrle använder Rittal-skåp för sin kraftelektronik. Systemen är modulbaserade och består av enskilda energilagringsmoduler som innehåller de enskilda battericellerna och ett batterihanteringssystem. De kan dimensioneras efter behov. Precis det antal energilagringsenheter som behövs plus en styrenhet installeras i ett VX25-apparatskåp.
Skåpsystem från marknadsledarna Rittal är välkända inom industrin och ökar förtroendet även för våra energilagringssystem på marknaden.
”Till skillnad från andra leverantörer använder vi inte vattenkylning för att kylning av våra energilagringselement, förklarar Schnakenberg. ”Därmed är de helt underhållsfria och mindre störningskänsliga.” De enskilda enheterna har endast kylflänsar på aluminiumkapslingen. Värmehanteringen sker då via kopplingsskåpets klimatsystem. Beroende på energilagrets storlek och miljöförhållandena på uppställningsplatsen kan då klimatlösningen anpassas. Även här har Commeo nytta av systempartnern Rittal: Eftersom skåp och klimatanläggningar kommer från en och samma leverantör passar allting perfekt ihop. ”Vi drar också fördel av de industritestade systemen när det gäller klimatregleringen”, säger Schnakenberg övertygat.
Världspremiär: Industriell UPS med litiumjonteknik
”Detta är världens första litiumbaserade avbrottsfria nödströmsförsörjning för industrianläggningar”, säger Michael Schnakenberg. UPS-enheten består av modulära energilagringselement som erbjuder en urladdningskapacitet på upp till 6 C (coulomb) med en effekt på 200 kW som får plats på mindre än en kvadratmeter. Prestanda i denna klass innebär att systemet kan upprätthålla strömförsörjningen till exempelvis Tiratex-förpackningslinjen från Windmöller & Hölscher fram till dess dieselgeneratorsystemet har kommit igång och kan ta över försörjningen.
Real-world test
Power cuts are something Windmöller & Hölscher, manufacturers of flexible packaging machinery, cannot afford. If their high-tech systems come to a standstill, hours of production downtime are the consequence. With the joint solution from Rittal and Commeo, however, such power cuts will be a thing of the past in the future. For example, Windmöller & Hölscher’s TIRATEX tape stretching system is supplied with uninterruptible power.