Apr 4, 2022

Rittal and Eplan at the “The Smarter E Europe” 2022

Energy systems of the future: faster planning and implementation

Energy transition needs pioneering solutions. The rapid transformation of energy systems requires time and cost-saving value creation processes in all areas, along with standardised and industry-tested systems. At “The Smarter E Europe” energy trade fair (11 – 13 May in Munich), Rittal and Eplan will be providing specific and practical examples that show how the engineering and installation of systems can be significantly accelerated and how network operators and project developers can benefit from improved cost efficiency. Solutions for e-charging infrastructures, energy storage, photovoltaic systems, hydrogen systems, and outdoor distributors for substations will be presented.

“The pressure on plant constructors and network operators has increased immensely. As a result, there is a demand for standardised, industry-tested, modular solutions that ensure maximum efficiency,” says Jan Oliver Kammesheidt, Vertical Market Manager Energy at Eplan.

In energy generation, transmission, storage, and consumption, Eplan and Rittal are presenting the latest solutions for every sector of the energy industry so that implementation saves time and costs. “The pressure on plant constructors and network operators has increased immensely. As a result, there is a demand for standardised, industry-tested, modular solutions that ensure maximum efficiency,” says Jan Oliver Kammesheidt, Vertical Market Manager Energy at Eplan.

“Rittal and Eplan support customers along the entire value chain, from engineering and semi-automated plant construction to plant operation. This way, we are actively shaping the transformation of energy supply together," adds Raphael Görner, Executive Vice President of Rittal’s Global Energy & Power Solutions Business Unit.

Modular kit for autonomous energy systems

The highlights at the trade fair booth include the new battery storage system from Tesvolt, installed in a Rittal VX25 enclosure system. Together, Tesvolt and Rittal have redeveloped the concept of climate control.

A complete energy supply system with hydrogen technology from H2 Core Systems is also implemented in a VX25 enclosure system. The modularly configurable system combines water electrolysis and fuel cells in one unit. Connecting an external hydrogen storage unit creates a self-sufficient energy system for short and long-term energy storage. It can be integrated into all existing photovoltaic, wind, or hydropower plants.

Rittal is presenting preconfigured configurations for AC distributors, particularly for PV plants. The solution in the AX compact enclosure is equipped with a weatherproof roof and a 185 mm busbar system for power distribution.

“Rittal and Eplan support customers along the entire value chain, from engineering and semi-automated plant construction to plant operation. This way, we are actively shaping the transformation of energy supply together,” says Raphael Görner, Executive Vice President of Rittal’s Global Energy and Power Solutions Business Unit.

Setting up a charging infrastructure quickly and securely

Rittal shows how standardised, reliable, and quickly implemented systems support the mobility revolution when it comes to charging infrastructure. The company offers suitable enclosure, climate control, and power distribution technology with a pre-designed system to set up charging parks. Rittal is presenting a back-end solution for a bus charging infrastructure with an example from its client SBRS, which is developing and commissioning fast chargers with a 150-kW output for e-buses.

In Zillmer’s ezy charge AC, a solution is presented directly for the charging point that relies entirely on the standardised Rittal AX enclosure series for efficient expansion. Moreover, Eplan and Rittal are using a demonstration project with the Lübeck University of Applied Sciences to demonstrate how a charging park’s local distribution network, including charging stations and energy storage devices, can be efficiently planned using Eplan software. EPLAN Cloud is deployed to manage all engineering steps, ranging from the initial project design through engineering to maintenance processes during later operation. This shows how mains connection and inverter technology can be put into operation quickly and safely with Rittal enclosure and climate control solutions.

Rittal is also demonstrating the diversity of its portfolio for outdoor applications: Customers can find the right solution for every installation site, from covered back-end systems to desert-based solar inverters.

Rittal ePOCKET – the digital wiring plan pocket

The sister companies are also presenting Rittal ePOCKET – the digital wiring plan pocket. A QR code on the enclosure permits access to the complete equipment and system documentation, including the digital twin in EPLAN Cloud, which is always up-to-date over the entire service life. Service and maintenance staff can directly access the wiring plans right on the system with a smartphone or tablet. This ensures quick troubleshooting in the event of repairs and maintenance.