ELECTRIFY YOUR SYSTEM

Charging infrastructure, energy efficiency and sector coupling

Take the right path to energy transition with strong partners

Energy consumption

Solutions for energy consumption

Energy transition does not end with the distribution and storage of electricity. Energy consumption also plays a major role and has several different considerations. For example, it is about efficient energy management, with which businesses, especially the manufacturing industry, can reduce power consumption. Sector coupling, or in other words connecting the electricity, heating, building, transport and other industrial sectors, is another important component of energy transition.

With regard to increasing e-mobility, it is crucial to make electricity available at many decentralised points: in charging parks, at home, at work or when shopping. In short, charging infrastructure is needed wherever the car is parked.

Innovative concepts with in the FLG group 

Integrated hardware and software solutions are increasing the pace of energy transition. Rittal is tackling these new issues together with its sister companies Eplan and GEC so it can digitalise and automate processes. In this way, it will be possible for even complex systems and tasks to be mapped with greater clarity and prepared for the future more quickly.

The most effective results are from best-practice examples based on many customer projects that have been undertaken. For example, there are pre-designed solutions for the planning and implementation of charging parks that the planner can easily access in electrical engineering with Eplan. The pre-configured project contains every detail, including standardised industrial hardware, and only calls for minimal customisation – time saving par excellence.

Your benefits at a glance:

  • Planning and implementation in record time – best-practice solutions exist and are available instead of elaborate new designs
  • First-class quality – error-free project planning with tried and tested solutions
  • Perfect synergy and co-ordination – hardware and software are perfectly matched to each other
  • Global application options through compliance with international standards and worldwide service
  • Forward-looking partners with new and innovative solutions for energy transition – for the competitiveness of your company

Typical solutions for charging infrastructure:

Baies outdoor

CS Toptec

Baie outdoor avec socle de transport de 100 mm et toit antipluie dépassant de tous les côtés. Parois latérales, paroi arrière et porte totalement doublées vers l'extérieur, l'ossature TS 8 complète...

Armoires électriques

Armoires juxtaposables VX25 en tôle d'acier

System Perfection. Les nouvelles armoires électriques juxtaposables VX25 en tôle d'acier offrent une qualité maximale et permettent une continuité des données en ingénierie, un faible degré de...

Coffrets électriques

Coffrets électriques AX

System Perfection. Le nouveau coffret électrique AX offre une qualité maximale et permet la continuité des données en ingénierie ainsi que la flexibilité et la sécurité lors du montage et de...

Habillage électrique

Baies outdoor

Les coffrets Outdoor sont spécialement prévus pour être implantés dans un environnement extérieur. Comme produit standard, Rittal propose des coffrets muraux CS et des baies New Basic CS disponibles sur stock. Les...

Distribution de courant

VX25 Ri4Power

TGBT fiable avec attestation de type pour machines, installations électriques et distribution de courant.

Success Stories.

Tritium

L’électromobilité pour tous

La disponibilité internationale et la qualité des produits Rittal étaient déterminantes pour la commande. La solution Rittal est entre autres mise en œuvre pour protéger les composants électriques sensibles des bornes de recharge contre les intempéries.

SBRS GmbH

Protégé contre la pluie et le soleil

À Fribourg en Brisgau des bus électriques roulent pour un climat parfait. Une infrastructure de recharge, qui offre une protection optimale contre les intempéries ainsi que l’accès des personnes, élaborée de la société SBRS GmbH avec des composants de...

Gemamex

Sofia – electric buses rapidly charged thanks to the VX25

Thirty electric buses are in service in the Bulgarian capital of Sofia. The charging infrastructure consists of Rittal VX25 enclosures, specially assembled into a three-unit combination for Gemamex, the manufacturer of the fast-charging stations.

Kölner Verkehrs-Betriebe/SBRS GmbH

Voll in 60 Minuten

Die Ladeinfrastruktur gilt als eine der großen Hürden auf dem Weg zur Elektromobilität. Auch der innerstädtische Busverkehr benötigt, wenn er auf E-Mobilität setzt, leistungsfähige Ladestationen. Wie diese aussehen können, zeigen die Kölner...