2017-08-28. Mississauga, ON - 10 hours of precise production work in 90 minutes, capacity to handle up to 3600 x2300 mm panels: Behold the magic of the Perforex!
Rittal Limited (www.rittal.ca), market-leading manufacturer of enclosures and thermal management of electrical, electronic and IT equipment, has stepped up the capabilities of their Mississauga Modifications Centre with the integration of the Perforex machine as part of the Rittal Automation System Plan. Rittal is always innovating and introducing ground-breaking technology like the Perforex machine, which is extremely precise, fully automated, and can be deployed for drilling, thread tapping, and milling when machining enclosures.
Rittal Automation System is a producer of machining centers for enclosure assembly, cutting centers, automatic assembly systems for terminal strips, assembly tables, and enclosure test units, into the overall Rittal organization. Rittal Automation Systems extends Rittal’s comprehensive range of solutions for panel building and switchgear engineering through key machining and handling technologies. Now with a comprehensive range of equipment available for professional workshop operation, from manual tools to sophisticated fully automated mechanical engineering, Rittal offers a comprehensive, one-stop portfolio for customers across the world.
With the integration of the Perforex into our Modifications Centre, we are pleased to offer our customers enhanced productivity by automating and streamlining manual modification and wiring processes. Our experienced staff in our state-of-the-art Modifications Centre are well equipped to modify our enclosures in record time, leading to cost-effective production and enhanced quality, while adding repeatability to processes and reducing lead-times for customers.
The Heart of the Automated System: Perforex
The Perforex machine enables 10 hours of panel production work to be completed in just 90 minutes. Perforex delivers not only time savings but increased accuracy and reduced waste with its CNC precision-capabilities. Perforex units call upon up to 20 tools in the magazine for operations including drilling tapping, milling and circular thread milling,
Perforex can handle clampable panels up to 3600×2300 mm, and since programming is faster than manual marking, the system is economically advantageous from a batch size of one. Perhaps most importantly, there are important design advantages inherent in Rittal enclosures that are amplified with the Perforex machining center.
Rittal offers Moteur du Cuivre a very versatile solution with its modification center capabilities and quick deliveries. Complemented by Rittal’s services such as 3D approval drawings and expert consulting, the complete enclosure solution is ideal for Moteur du Cuivre.
Adds Austin Brennan, President, House of Electricals, a valued distributor of Rittal Limited, who has set up an exclusive website that highlights the advantages of the Perforex machine, “The Perforex machine offers faster throughput, higher efficiency, greater precision, less waste and lower costs to our customers, while boosting their corporate image through unique, customized designs”.
Rittal is the only company in the world able to deliver an end-to-end solution from a single source, with seamless integration and specific advantages every step of the way.
About Rittal Limited:
Rittal Limited, headquartered in Mississauga, Ontario, is the Canadian Subsidiary of Rittal GmbH & Co. KG, Germany, which is the world's leading system supplier for enclosures, power distribution, climate control, IT infrastructure and software & services. Founded in 1961, Rittal is now active worldwide with 10 production sites, 63 subsidiaries and 40 agencies. With over 11,000 employees worldwide, Rittal is the largest company of the proprietor-run Friedhelm Loh Group of Haiger, Germany.
www.rittal.ca and www.friedhelm-loh-group.com.
Media Contact:
Marketing- Rittal Limited Canada
marketing@rittal.ca